I am new to LP. Testing a code for a scope found at "http://www.msp430launchpad.com/2010/12/njcs-launchscope-launchpad-oscilloscope.html" It works, but use p1.3 (A3) as input.That pin has a pulldown resistor. (have searched the forum, but found no answer) To use p1.3 as analog input, is the solution to use an op.amp. between p1.3 and the analog signal or are there other pin on the LP that could be used? An opamp can also "clip" the signal when to high or neg.