Other Parts Discussed in Thread: MSP-TS430PN80A, MSP-TS430PN80USB
Is there an 80-pin target board for the 5418?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP-TS430PN80A, MSP-TS430PN80USB
Is there an 80-pin target board for the 5418?
Terry,
Unfortunately no, the 80 pin target boards only support:
My suggestion for the customer would be to develop using the MSP4305438 Experimenter's Board: http://www.ti.com/tool/msp-exp430f5438
Austin is right.
For testing/evaluation, the 5438A 100-pin target board can be used with a 5419A processor. The 5419A and the 5418A are identical except for the additional ports and the two additional USCI modules. So if these additional pins are not used, the software as well as any attached hardwar ecan be later used 1:1 on a PCB for the 80 pin device.
**Attention** This is a public forum