Part Number: MSP430F5510
Hello, I have:
- TI's CCS12.8.1
- TI MSP-TS430RGC64USB dev kit with a MSP430F5510 cpu
- TI MSP430-FET430UIF debugger connected via ribbon cable
- Known working firmware that communicates to host PC via USB and CCS project.
- This firmware enuemerates itself as HID KB with the host PC
Last week I could either update the target CPU with firmware or debug it with breakpoints etc sucessfully but as of today the same setup mysteriously no longer functions.
When I either try Run>Load>... or Run>Debug>.... from CCS the following appears:

and debuggers green "power" led & red "mode" led are lit, but are followed with these messages:

What was a functioning debugger has suddenly decided to stop recognising a functioning MSP430 devkit which is still running the firmware from last week.
Something odd has happened to the debugger without human intervention!
Any Ideas?
Thanks
Ps I have tried different USBcables, turning thing off/on again etc