Part Number: MSP430FR4133
Hello,
I am using the etl cpp library (https://www.etlcpp.com/home.html), specifically `etl::bitset` (https://www.etlcpp.com/bitset.html).
When I am compiling my code, I get the following error from the compiler:
[0]**** Build of configuration 'Debug' for project 'Thermometer' ****
[1]"C:\\ti\\ccs2031\\ccs\\utils\\bin\\gmake" -k -j 16 all -O
[2]Building file: "C:/Projects/Thermometer/src/targets/msp430/hal_button_msp430.cpp"
[3]Invoking: MSP430 Compiler
[4]"C:/ti/ccs2031/ccs/tools/compiler/ti-cgt-msp430_21.6.1.LTS/bin/cl430" -vmspx --use_hw_mpy=none --include_path="C:/Projects/Thermometer/src/" --include_path="C:/Projects/Thermometer/src/app" --include_path="C:/Projects/Thermometer/src/lib/etl/include" --include_path="C:/ti/ccs2031/ccs/ccs_base/msp430/include" --include_path="C:/Projects/Thermometer/src/targets/msp430/CCS-Workspace/Thermometer" --include_path="C:/Projects/Thermometer/src/targets/msp430/CCS-Workspace/Thermometer/driverlib/MSP430FR2xx_4xx" --include_path="C:/ti/ccs2031/ccs/tools/compiler/ti-cgt-msp430_21.6.1.LTS/include" --advice:power="none" --advice:hw_config=all --define=__MSP430FR4133__ --define=DEPRECATED -g --printf_support=minimal --preproc_with_comment --preproc_with_compile --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --obj_directory="Hal" "C:/Projects/Thermometer/src/targets/msp430/hal_button_msp430.cpp"
[5]INTERNAL ERROR: C:\ti\ccs2031\ccs\tools\compiler\ti-cgt-msp430_21.6.1.LTS\bin\acpia430.exe experienced a segmentation fault
[6] while processing function (unknown or file scope) file C:\Projects\Thermometer\src\lib\etl\include\etl\private/bitset_new.h line 1874
[7]This is caused by a defect in the TI EABI C/C++ Parser.
[8]TI Customer Support may be able to suggest a workaround to avoid this.
[9]Upgrading to the newest version of the compiler may fix this problem.
[10]Contact TI in the E2E support forums at http://e2e.ti.com under
[11]"Development Tools", "TI C/C++ Compiler". See the link titled
[12]"Submitting an issue".
[13]We need to see this ENTIRE error message and a complete, reproducible
[14]test case including ALL of the command-line options.
[15]Include the .pp file created by option --preproc_with_comment
Here is the .pp file, saved with extension .txt because I could not upload it otherwise: hal_button_msp430.txt
How can I work around this issue?
Thanks for the help!
Cheers
Emile