Hello,
I just bought the Launchpad and I was doing some simple tests with it. I decided to test the on-board push button in P1.3 and I think it is not working properly. I wrote a simple code to turn on the on board LED when the push button was pressed. The push button doesn't work when pressed. Only if I touch the P1.3 pin connector or the push button's solder under the board that the LED is lighted.
Is this something wrong with my code or with my board? If the latter, there is a way to correct this?
Thanks,
Daniel K. Franch