Part Number: MSP430FR5969
I previously implemented a PWM algorithm on the MSP430FR5969 microcontroller, using timer A1 as the "Base". In this endeavor, the example provided by TI under the folder lab_06d_simplePWM in the workshop was quite helpful. We now are on a mission to implement the algorithm with PDM via SPI and DMA. The question I have: are there any sample code that you can provide that may be useful? Specifically setting up the DMA, SPI, maybe a bit of the algorithm itself (Ping-pong version if available) would be best. The example, if in existence, does not have to be necessarily for the MSP430FR5969, any example for any TI microcontroller would be helpful. Thx in advance for your time.
Best Regards,
Ramin Sinaee
L3Harris Corporation