This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G5187: Generating a second clock out of the device

Part Number: MSPM0G5187
Other Parts Discussed in Thread: SYSCONFIG

I need a clock input to another device on my system, and instead of creating yet another clock, I was hoping I could use the MSPM0G5187 to generate a clock.  The frequency, jitter, and such is not that critical, anything over 1MHz will work.  It's just to one other chip, so drive isn't critical.

I'm already using the CLK_OUT pin for another clock, so I can't use that.

Looking at the chip, I think I can use a countdown timer that automatically reloads to trigger an event.  It looks like, with a 32MHz clock to the timer, I can trigger the event at 16MHz.  Maybe 32MHz.

Then that event can toggle a GPIO pin, so I can get an 8MHz (maybe 16MHz?) clock out of the GPIO pin.

Does all this look correct?

Thanks,

-corey

**Attention** This is a public forum