Part Number: LP-MSPM0C1104
Hello, I am using the LP-MSPM0C1104 to explore the MSPM0C system. I am trying to flash and debug a very simple code and I get this error in CCS 20.5.0 "No matching COM port found" when I try to flash the LaunchPad board.

I have correctly installed the latest version of CCS 20.5.0.28_1.11.0 and the project that I am trying to upload was build without errors.
The XDS110 COM ports are visibile on the Device Manager on my PC, as you can see in the image below:

Also in the targetConfigs file, it seems that the connection with the board is OK:

Do you have any suggestion on how can I overcome this issue?
Thanks for the support.
F.A.