This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553: msp430g2553 debugging issue

Part Number: MSP430G2553
Other Parts Discussed in Thread: MSP-FET

I am experiencing debugging issues: as soon as I insert a breakpoint, the system resets. The same thing happens if I press the 'Pause' button. I have tried various settings without success. I have used this controller for years, but I am now using a computer equipped with an Intel Core Ultra 7 258V and Windows 11, which seems to be causing these problems.

Additionally, the MSP-FET is a newer model compared to the one I used previously at another company. There was a brief moment when everything functioned correctly, but then it stopped working again. Please note that I program exclusively in Assembly.

can yuo help me to set correct the ode composer ? 

Best REgards 

Luigi 

**Attention** This is a public forum