This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3519: The MSPM0G3519 cannot write data to the DATAFLASH using the FLM firmware in the Keil package.

Genius 14480 points

Part Number: MSPM0G3519

Hello.

I have encountered a problem. I used the MSPM0GX51X_DATA_16KB.FLM driver in Keil Pack to program the DATAFLASH of MSPM0G3519. The address controlled by this FLM is 0. So I manually changed it to 0x41D00000. However, after erasing, the programming failed and the return value was 1. Could you tell me if this is a problem with the FLM? If so, could you provide the latest FLM driver file?
thank you

**Attention** This is a public forum