I would like to use the software described in SLAU320C and SBW connection to an MSP430G2211but I am confused about the connection and software. The software function StartJtag clears and then sets the target JTAG TEST signal, then runs an initiation sequence using SPWTDIO and SBWTCK. But on the MSP430G2211, TEST and SBWTCK are the same pin. Do I in effect OR these two signals out of the REP430F, do I leave TEST unconnected, or what?