Other Parts Discussed in Thread: MSP430G2432
I recently switched from an older version (don't remember which) to CCS 5.1.0.09000 on windows 7.
I ran in to trouble with one old program because the chip started to pull some pins high (program wasn't changed)
I used Grace in the old CCS version, and I am using the built in version of CCS 5.1.0.09000
Using the debugger I discovered that P2OUT is apparently initialized at a value of "1011111" after reset.
In the old version I also noticed that P2SEL was initialized at "11000000"
Is it necessary to initialize this at the beginning of each program? In Grace these registers are set to 0 , so why does grace not take care of this initialization if needed?
Are there any other changes like this that I can expect?
This application drives a high power switch, so any sudden changes in behavior could be dangerous.