This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3519: MSPM0G3519 : 80 MHz configuartion Example code causing Device Mismatch Issue

Part Number: MSPM0G3519

Hi,

I am using MSPM0G3519 launchpad for development. After flashing the sysctl_mclk_syspll_LP_MSPM0G3519_nortos_ticlang example code, further flashings are not working.
Error thrown is : Device connected is different.
Attaching the error message screenshot:
Screenshot from 2026-04-24 16-39-42.png

 

CCS Version : 1281
SDK Version : mspm0_sdk_2_10_00_04

**Attention** This is a public forum