Other Parts Discussed in Thread: MSP430F2274
Hi,
I'm trying to configure the general purpose op-amp inside the MSP430F2274. All pins should be connected externally.
I want to make this oscillator (3.1):
http://www.ti.com/lit/an/slaa363a/slaa363a.pdf
This is my code:
void main (void)
{
/*
P2.0 = non inverting in
P2.1 = OA OUT
P2.2 = Inverting in
*/
P2SEL = 0;
P2DIR = BIT0;
// Set up Op Amp 0
OA0CTL1 = OAFC_0; // OAFC0 = 0 General Purpose Op amp
OA0CTL0 = OAN_1 | OAP_0 | OAPM_2 | OAADC0 ; // Inverting pin connected to OA0I1; Non inverting pin connected to OA0I0; Out connected to A1 A3 A5; Medium selw rate
ADC10AE0 = BIT0 | BIT1 | BIT2; // P2.0-OAI0, P2.1-OAO, P2.2-OAI1 Analog settings
//Main
while (1)
{
}
}
I don't get why it doesn't work properly. Can you help me please?