Other Parts Discussed in Thread: MSP430F5172
Hi,
I am using an MSP430F5172. What is the best practise for getting lowest noise measurements from the ADC10? I don't need the internal reference for accuracy, VCC would be fine. But I suspect noise from the supply voltage could induce errors on the ADC10 measurement. Does it make sense to generally use the internal reference? I don't mind the extra supply current for the REF module. Using a 2.5V reference however would mean a reduced input voltage range (compared to a 3.3V VCC), so errors on the analog path play a bigger role.
Regarding the temperature diode: The manual does not mention it, but it seems to work only when REF is swiched on. Is it important which reference level to use?
- Regards