The most frequent problem we run into programming boards is they have the error:
MSP430: Error connecting to the target: Unknown device
We haven't been able to trace this error - some boards program fine, some will never program, others will program sporadically. We use the Spy-Bi-Wire on our board with a 47kohm 1% pullup to Vcc and a 2.2nF 10% capacitor to ground, like it says in the app note.
Do the resistor and capacitor need to be close the the input pin on the MCU? Has anyone else run into this repeatedly?