Part Number: MSP430G2553
Other Parts Discussed in Thread: ADS7049-Q1, MSP-EXP430G2ET,
Hello,
I am using the MSP-EXP430G2ET LaunchPad with the MSP430G2553 MCU and an external ADS7049-Q1 12-bit SPI ADC for temperature sensing.
The ADS7049-Q1 is configured with:
-
External reference voltage = 2.5 V
-
SPI interface using SCLK, SDO, and CS
-
ADC input range = 0 V to 2.5 V
I have a few questions regarding the hardware interface and software setup:
-
Since the ADS7049-Q1 operates with a 2.5 V supply/reference, should the SPI signals (SCLK, SDO, and CS) also be limited to 2.5 V?
-
The MSP430G2553 LaunchPad is powered from USB and its GPIO pins operate at approximately 3.3 V. Can the ADS7049-Q1 safely interface directly with these SPI signals, or is level shifting required to avoid damaging the ADC?
-
Is there any recommended TI example code or driver for interfacing the ADS7049-Q1 with the MSP430G2553 using the hardware SPI peripheral?
-
For software development, should I use Code Composer Studio (CCS) for the MSP430G2553 LaunchPad?Or any MSP430 software i need to download tell all. If so, could you please recommend the appropriate CCS version and any required MSP430 SDK or support packages?
-
Are there any recommended hardware or software considerations to ensure accurate conversion results and correct calculation of ADC counts when using a 2.5 V reference?
Thank you.