This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3519: MSPM0G3519: Error connecting to target when debugging

Part Number: MSPM0G3519
Other Parts Discussed in Thread: UNIFLASH

Hello , 

I am facing an issue in connecting my target MSPM0G3519 with the debugger (trace 32 )

 

Error Message shown in both debuggers: 

T32:

When connected with T32 debugger  getting this error: 

 

 

CCS STUDIO :

When connected to CCS studio :

Error connecting to the target:  Connection to MSPM0 core failed.  Possible root causes:

1) Debug access within NONMAIN was disabled or enabled with password.

2) Peripheral mis-configuration (e.g improper watchdog or clock).  To see a more detailed diagnostic of the issue, please press the 'Read boot diagnostic' button.

 

When Clicked Read Boot diagnostics button :

 

CS_DAP_0: Device diagnostic read = 0x00000036

CS_DAP_0:

Possible root causes could be one or multiple of the following:

1) Invalid CRC configuration

2) Invalid BCR configuration

3) Invalid BSL configuration

 

Possible recovery method:

1) Perform a DSSM factory reset

2) If method one does not work please remove power, hold nRST low, connect the device while nRST is held low, and then perform a DSSM factory reset

 

Questions:

1. Is there any recovery method for this situation?
2. Based on the diagnostic value 0x00000036, 

  • Hi Abhilash,

    You could refer the 7.1 sector of MSPM0 MCUs Development Guide (Rev. G) for MSPM0 factory reset.

    Notice it should based on XDS110 debugger + Uniflash/CCS. The XDS110 embedded in MSPM0G3519 launchpad could also be used in this case.

  • Hi Pengfei Xie,

    We tried this method, but the board is not up 

    Unable to connect the board via CCS Studio, also getting the same diagnostic report as above 

    CS_DAP_0: Device diagnostic read = 0x00000036

    CS_DAP_0:

    Possible root causes could be one or multiple of the following:

    1) Invalid CRC configuration

    2) Invalid BCR configuration

    3) Invalid BSL configuration

    Possible recovery method:

    1) Perform a DSSM factory reset

    2) If method one does not work please remove power, hold nRST low, connect the device while nRST is held low, and then perform a DSSM factory reset

  • Please have a look on below code which might have affected the board , since board was in running reset mode before going debug port timeout in t32 

    Please have a look on below code which might have affected the board , since board was in running reset mode before going debug port timeout in t32 :
    
    FUNC(void, BSWM_APPL_CODE) Eb_Intgr_BswM_WaitMemDriverReady(void)
    {
    #if defined(BASE_MEMIF_ENABLED)
    #if (BASE_MEMIF_ENABLED == STD_ON)
    MemIf_StatusType status = MEMIF_UNINIT;
    #endif
    #endif
    uint16 iterCount = 0U;
    
    /* Loop until Fee reaches IDLE so it has time to write virtual-sector headers
    * on blank data flash (first boot / after sector erase). Stop immediately on
    * IDLE to avoid triggering spurious background compaction.
    * Safety cap: 200 iterations prevents an infinite loop if Fee gets stuck. */
    do
    {
    #if defined(BASE_FEE_ENABLED)
    #if (BASE_FEE_ENABLED == STD_ON)
    Fee_MainFunction();
    /*
    FLS_MAIN_FUNCTION_DEFINE is configured in McalExt and will be generated in Platforms_Modules.h file
    e.g. #define FLS_MAIN_FUNCTION_DEFINE Fls_17_Pmu_MainFunction()
    */
    
    #ifndef _X86_
    /* MemAcc_MainFunction(); */
    #endif
    FLS_MAIN_FUNCTION_DEFINE;
    #endif
    #endif
    
    #if defined(BASE_FEE_ENABLED)
    #if (BASE_EA_ENABLED == STD_ON)
    Ea_MainFunction();
    Eep_MainFunction();
    #endif
    #endif
    
    #ifndef _X86_
    status = Fee_GetStatus();
    #else
    status = MemIf_GetStatus(0);
    #endif
    iterCount++;
    } while ((MEMIF_IDLE != status) && (iterCount < 200U));
    
    

  • Hi Abhilash,

    Two quick question here:

    • Do you use NONMAIN in your application?
    • Is this connection issue follow with your firmware or it follow a specific hardware board?

**Attention** This is a public forum