Other Parts Discussed in Thread: MSP430F149
I am trying to use the IAR kickstart software to program a FET430P140 tool using the parallel interface adapter, however, the settings in IAR Workbench support LPT 1, 2, or 3 at the standard ISA addresses of 0x378, 0x278, or 0x3bc respectively. Device manager shows that my parallel port is addressed at 9800 - 9807. Is there a way to either change the IAR settings to seek the parallel port at 9800 or change the I/O range of the parallel port to one of the standard ISA addresses? My configuration is below. Due to ACPI, Windows does not allow me to make any changes under the Resources tab in Device Manager for the address settings. If I am better off using a different software instead of IAR that isn't limited to the standard ISA addresses, I could also try that. I have found that the PCI Bus under System Devices seems to be occupying those ISA addresses in the I/O Range of 0000 - 0CF7 (hexadecimal).
Software: IAR Kickstart Embedded Workbench 5.40.3
TI Hardware: MSP-FET430P140 w/ MSP430F149 and TI FET Parallel Interface Adapter
Computer Hardware: Siig Parallel PCI card model JJ-P11012-S6
OS: Windows 7 Professional 64-bit
Regards,
Anthony