This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3107-Q1: PA1 PWM Function Missing Despite Datasheet Support

Part Number: MSPM0G3107-Q1
Other Parts Discussed in Thread: SYSCONFIG

According to the M0G3107QPMRQ1 datasheet, PA1 supports PWM output through TIMA0 Channel 1 and TIMG8 Channel 0. However, when configuring the pin in the software (SysConfig), PA1 does not appear as an available timer/PWM pin, whereas PB26 is available for timer configuration. Could you clarify why PA1 cannot be configured for PWM despite the datasheet indicating that it supports these timer functions?

**Attention** This is a public forum