Other Parts Discussed in Thread: MSP-TS430PW28
I'm trying to debug an out-of-the- box configuration of an MSP-FET430UIF with an MSP-TS430PW28 (Rev.3.1) eval board from the same kit.
The IAR Workbench message is "Fatal error: Could not find device (or device not supported) Session aborted!"
I'm trying to use the Mode and Power LEDs on the UIF to isolate the problem to either the computer-to-UIF path (including the USB driver set-up or the Workbench options) or the UIF-to-target path.
Searched many manuals but couldn't find a description of the proper and erronous behaviour of these LEDs, both with the targe connected or with it disconnected.
In my case, when I get the error message both the red Mode LED and the green Power LED are lighted.
Does anyone know where the operation of these LEDs is described or have a discription of what they should be doing?
Is there a better way I should be trying to isolate the problem than trying to understand these LEDs?