Part Number: MSPM0G3218-Q1
Hello TI,
I am using a timer to trigger an ADC, which has two channel config and a repeat Sequence config, my current problem is, that the time between timer EVENT Trigger and actual MEMRESIFG interrupt is much longer than expected. So far I use SCOMP0=0x30 (32MHz) for my first MEMRESIFG and the corresponding conversion time. I should have around 1.7µs but get ~9µs.
In between the Timer trigger (yellow) and Memres interrupt (red) I do nothing but wait for the ADC interrupt and set GPIO in ISR. So far I think I made the right config for ADC and timer because I had it already running fine on another MSP.
Thanks in advance