This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sampling sine wave to detect zero crossing



Hi,

          I need to sample a rectified sine wave of 230V, 50Hz to detect its zero crossing .  but I am finding it difficult to continuously sample it. The code is given below:

void main(void)
{

WDTCTL = WDTPW + WDTHOLD; // Stop WDT
BCSCTL1 = CALBC1_8MHZ; // Set range
DCOCTL = CALDCO_8MHZ;
P1DIR |= BIT0;
P2DIR |=0xF8; // Set ports P2.0/1/2 to Input Direction
P2SEL |=0x07; // Select Ports P2.0/1/2 as analogue input function


// Configure the Timer_A in order to trigger the ADC10

TA1CCTL0 =CCIE; // Enable the Timer_A interrup
TA1CCR0 = 98; // Set Timer_A Capture/Compare Registor to TA_Prd
TA1CTL = TASSEL_2 + MC_1; // Select Sub_system Master Clock SMCLK as source of trigger signal
// Select Up_mode, the timer_A counts up to TACCR0

// ADC10 COnfiguration

ADC10CTL0 =ADC10ON + MSC; //ADC ON, Reference Voltage to 2.5 V and select Up-mode
ADC10CTL1 = INCH_1 +CONSEQ_2; // Select A1 as input channel, repeat single channel as conversion sequence
ADC10DTC0 = ADC10CT; // continuous data transfer


for (;;){
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
__bis_SR_register(CPUOFF + GIE); // LPM0, ADC10_ISR will force exit
if (ADC10MEM == 0x0000) {
                                 
 // some code    			

}
}

}

// Timer A0 interrupt service routine
#pragma vector=TIMER1_A1_VECTOR
__interrupt void Timer_A1(void){

_bis_SR_register_on_exit(CPUOFF);

}


  • Why don't you just use a Schottky diode and a resistor.  This will generate a pulse at the zero crossing point, and then feed that into an interrupt.  Zero MIPS.

    But if you have to use software, then set up the ADC to generate an interrupt after conversion.  Check the value in there.  You don't need a timer at all.

**Attention** This is a public forum