Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1105: Will using high Precision Vdd improve internal reference performance?

Part Number: MSPM0C1105

Hello, 

In system being designed a high accuracy 3.3V as well as a lower voltage high accuracy reference are needed. 

My question is will the accuracy of the internal voltage reference improve if a precision source is used for vdd?  If so Is this quantifiable?

 

Thank you, 

Joseph Scherphorn

Will using high Precision Vdd improve internal reference performance?

  • I don't think so, it is set by the internal reference. You can provide an exetrnal reference if you want.

    A high precision Vdd will prevent whatever power-supply variation might be present, it it is usually second or third order effects.

  • Here are the Ref specs:

    Note that the supply rejection is over 40 dB, so a precision VDD is not going to help much.

  • Hi Joseph,

    As Keith has pointed out, a precision voltage source will not have a significant effect on the accuracy of the internal VREF.

    If your system requires a higher accuracy VREF, I would suggest using an external reference.

    What kind of accuracy are you targeting? What is the application?

    Best,

    Owen

**Attention** This is a public forum