Part Number: MSP430F5325
Hi,
I want to improve ADC performance of MSP430F5325.
(1) In which applications is it recommended to support the internal reference with an external capacitor, example 100pF at VREF+(P5.0) ?
(2) Could you please confirm the follwing register settings?
REFCTL0 |= REFON; // Internal Reference ON
...
REFCTL0 &= ~REFMSTR; // Reset REFMSTR to hand over control to ADC ref control registers
ADC12CTL0 = ... + ADC12REFON;
P5SEL |= BIT0; // disables the output driver of P5.0 (VREF+)
ADC12CTL2 |= ADC12REFOUT; // connect internal VREF to pin VREF+
Best regards Joerg