Part Number: MSPM0G3107
Other Parts Discussed in Thread: SYSCONFIG,
I would like to provide an additional update regarding the issue.
PA18 is connected to the shunt sensing circuit on our hardware and is configured as an ADC analog input in the application. We are using this pin for shunt voltage/current measurement.
As PA18 is mentioned as the BSL Invoke pin in the MSPM0G3107 documentation, could you please confirm whether any additional hardware precautions, SysConfig settings, or software configuration changes are required when PA18 is used as an analog input?