According to the Tables 15-4 + 15-5 of the MSP430Fx2xx Users Guide Max TX error and Max RX error is defined as a negative and a %, please clarify.
For example in Table 15-5, for BRCLK of 16,000,000 / Baude Rate of 460800 / Max. TXError −2.1 (?) / Max TX Error[%] 4.8 (?) / Max. RX Error −2.5 (?) / Max RX Error [%] 7.3 (?). Please clarify, what is a negative error and define Error %.
-Tom-