UNIFLASH: Consult MCU Programming Method via Uni-Flash Bootloader Option

Part Number: UNIFLASH
Other Parts Discussed in Thread: MSPM0G3519, MSPM0G3507

Dear  TI ,

Currently, I am using UniFlash and selecting the Bootloader option to program the MSPM0G3519 MCU via UART.

Therefore, I removed the SWD connection on the EVM, as shown in the attached picture.

In UniFlash, I selected MSPM0GX51X (Bootloader) and loaded a .bin file or .out file.
Then I selected the UART interface, such as COM10. I also tested COM9.

However, the programming always fails, as shown in the screenshot below.

The same procedure works successfully on the MSPM0G3507, so I would like to confirm whether there are any additional settings or differences when using the bootloader to program the MSPM0G3519 via UART.

Thank you.

 

**Attention** This is a public forum