pls can anyone help me in changing the demo code to sample and transmit the ECG signal. the ADC program has been used thrice in demo_ED.C file whereas i am confused as how to use it for a continuous analog signal.
while (1)
{
volatile long temp;
int degC, volt;
int results[2];
SMPL_Ioctl( IOCTL_OBJ_RADIO, IOCTL_ACT_RADIO_SLEEP, "" );
__bis_SR_register(LPM3_bits+GIE); // LPM3 with interrupts enabled
SMPL_Ioctl( IOCTL_OBJ_RADIO, IOCTL_ACT_RADIO_AWAKE, "" );
BSP_TOGGLE_LED2();
ADC10CTL1 = INCH_10 + ADC10DIV_4; // Temp Sensor ADC10CLK/5
ADC10CTL0 = SREF_1 + ADC10SHT_3 + REFON + ADC10ON + ADC10IE + ADC10SR;
for( degC = 240; degC > 0; degC-- ); // delay to allow reference to
settle
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
__bis_SR_register(CPUOFF + GIE); // LPM0 with interrupts enabled
results[0] = ADC10MEM;
ADC10CTL0 &= ~ENC;
ADC10CTL1 = INCH_11; // AVcc/2
ADC10CTL0 = SREF_1 + ADC10SHT_2 + REFON + ADC10ON + ADC10IE + REF2_5V;
for( degC = 240; degC > 0; degC-- ); // delay to allow reference to
settle
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
__bis_SR_register(CPUOFF + GIE); // LPM0 with interrupts enabled
results[1] = ADC10MEM;
ADC10CTL0 &= ~ENC;
ADC10CTL0 &= ~(REFON + ADC10ON); // turn off A/D to save power
// oC = ((A10/1024)*1500mV)-986mV)*1/3.55mV = A10*423/1024 - 278
// the temperature is transmitted as an integer where 32.1 = 321
// hence 4230 instead of 423
temp = results[0];
degC = ((temp - 673) * 4230) / 1024;
if( tempOffset != 0xFFFF )
{
degC += tempOffset;
}
/*message format, UB = upper Byte, LB = lower Byte
-------------------------------
|degC LB | degC UB | volt LB |
-------------------------------
0 1 2
*/
temp = results[1];
volt = (temp*25)/512;
msg[0] = degC&0xFF;
msg[1] = (degC>>8)&0xFF;
msg[2] = volt;
if (SMPL_SUCCESS == SMPL_Send(linkID1, msg, sizeof(msg)))
{
BSP_TOGGLE_LED2();
}
else
{
BSP_TOGGLE_LED2();
BSP_TOGGLE_LED1();
}
}
}
if i use results[ ] array to be a empty set then wil it work for an continuous analog signal.
pls kindly help me!