MSPM33C321A-Q1: Scope plotting with Code Composer Studio

Part Number: MSPM33C321A-Q1

Hi, does CCS support following type of scope plotting like the examples shows with X2C Scope:

X2C Scope allows to plot up to 8 global variables by adding an update timer in the X2CScope_Update() function. The data are stored to a buffer and can be triggered by e.g. PWM-Motor-Interrupt. The Sample Time Factor which sample (n-Sample) will be plotted. By this feature it's possible to record and plot  a large time window.  The plot woindow (GUI) can be defefined as needed (y/x plot).

See the image attached for more details.

Does CCS have such a feature or even more advX2C-Plot.pnganced features?

Please let me know 

**Attention** This is a public forum