This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

After factory reset - Wireless connectivity problem

I used Fet-Pro430 to reset the ez430-chronos to factory setting.  After I did that, my wireless connectivity is not working?  Is that got something to do with the 433, 868, 915 MHz source codes? I used the 915MHZ code for reset.

Thanks in anticipation,

Shailesh

  • Hi!

    I'm facing the same situation.

    First, I've tried to update my chronos's firmware thru wireless, but i've got an error message and it was impossible to try again. Then I opened the watch and made a wired download, using the debug interface and FET-Pro430 software.

    After this I'm trying to comunicate in ACC mode and nothing happens. I see the AP's led flashing in a very low rate (1s on, 1 or 2s off) and the watch automatically ends the ACC mode. Did I do something wrong, during firmware download? I've used the following settings:

    uController: CC-430F6137

    Power: 3,3V

    FIle: eZ430_Chronos_ Datalogger_915MHz_1_5.txt

    I tried to erase only user memory, and then all memory.

    Can someone help me with this situation?

    (PS: My model is 915Mhz)

    Thanks in advance!

    Fernando Ginez da Silva

    _________________________________

**Attention** This is a public forum