Other Parts Discussed in Thread: MSP430F248
Hi,
I am using MSp430F248 in my circuit and the problem is 12-bit ADC readings are little off approximately by 10 to 15 counts. It is two plane board with Digital ground and Analog ground tied together. So basically there is only one ground. I added 10uf 6V caps to pin 1 and pin64 i.e DVCC and AVCC as mentioned in user guide document. I calculate the counts that I should expect by measuring the scaled down voltage that is being input to the ADC pins and using the formula given in datasheet i.e Vadc = Vin * 4095 /vref+. I am using internal Vref+ -2.5V and Vref- = 0V. Can someone please give me some idea what could be the reason for it. I am really having tough time with this.
Ali.