This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5739: Using FRAM



So I'm trying to write some code where the actual code section is stored in the SRAM, but the global variables are stored in FRAM.  I'm using the IAR Embedded Workbench IDE which means I'm going to need to change how the linker file is setup, but I can't figure what I actually need to change.  I'm also not sure if I need to put anything special in the code to make sure that the variables are put into the proper space.

Please help me out. :)

Thanks.

**Attention** This is a public forum