On page 20-5 of SLAU144F, following points are given. What is meaning of highlighted text.
1.The eight external and four internal analog signals are selected as the channel
for conversion by the analog input multiplexer. The input multiplexer is a
break-before-make type to reduce input-to-input noise injection resulting from
channel switching as shown in Figure 20--2. The input multiplexer is also a
T-switch to minimize the coupling between channels. Channels that are not
selected are isolated from the A/D and the intermediate node is connected to
analog ground (VSS) so that the stray capacitance is grounded to help
eliminate crosstalk.
The ADC10 uses the charge redistribution method. When the inputs are
internally switched, the switching action may cause transients on the input
signal. These transients decay and settle before causing errant conversion.
2. on page 20-6,
The ADC10 internal reference generator is designed for low power
applications. The reference generator includes a band-gap voltage source
and a separate buffer.The current consumption of each is specified separately
in the device-specific data sheet.
What are these two-> band-gap voltage source & separate buffer & diff in their function.
3. On page 38 of SLAS735C, sevaeral error are given: Integral linearity error,Differential linearity error ,etc. What is their meaning.
4. What is error in ADC10. is it +-1LSB.