Hello
I am trying to get the MSP430FE427A working in slave mode at a speed of at least 2MHz. I have been able to get it to work correctly to 500Khz but beyond that I am getting corrupt data. The processor is running at 8 MHz. Would anyone have an ideas on how to get this interface to work faster? Basically, when I receive a command, I transfer the bytes from memory to TXBUF0. There is no other processing involved.
Could this be an upper limit for this microcontroller in SPI slave mode?