Hi Lisa,
Now, i have a fresh problem, i have installed IAR(5.40.3), CCS 4(4.1.2.00027) and
CCS 5(Version: 5.1.1.00031 )
on my machine. I was using CCS 4(Drive C) without any hassle all these days,
recently i installed both CCS 5 and IAR(Both on drive D).
First i used only IAR for burning my code to the MCU. Very rarely i would use both CCS 5 and IAR.
The Problem: Now whenever i burn a program with CCS 5, the calibration constants are getting erased.
I have selected the "Erase main, info and protected info mem" option under the MSP430 properties.
Then i ran the "msp430x261x_dc0_flashcal.c - DCO Calibration Constants Programmer" from
examples code and now whenever i use IAR, everything works fine.
1)Why is this happening??
2) Should i stick to only IAR??
3) After i started using CCS 5, when i occasionally try to use CCS 4 it gives
an error "FET already in use"
or some error, but it refuses to load the program, please let me know the reason for this behaviour?
Phew.. finally, i would be very much grateful if you could help me out. Thanks.
best wishes
janmay