Other Parts Discussed in Thread: MSP430F155
hi all am using msp430f155 controller for my project.. and i tried to do a adc and outed in dac.here i used external referencre 3v for adc and dac..here below its my code....and i try to check the adc value by outing the first channel ADC value directly to the DAC.. and i put the break point at the end of the program. and i monitored the a1 chanel decimal value for my adc input..
here my input voltage is =1.060V for this input the Nadc should be =1449..but if i watching at break point am getting .1439,1452,1463 like that so each time while i excute am getting 15 to 20 value difference because of this am getting error about 4mv in dac output.. how can i minimize this error..and i need to know the reason for this..
#include <msp430x15x.h>
#define Num_of_Results 10
static unsigned int A0results[Num_of_Results]; // These need to be global in
static unsigned int A1results[Num_of_Results]; // this example. Otherwise, the
static unsigned int A2results[Num_of_Results]; // compiler removes them because
static unsigned int A3results[Num_of_Results]; // they are not used
static unsigned int A4results[Num_of_Results]; // they are not used
static unsigned int Arefresults[Num_of_Results]; // they are not used
unsigned int A0 = 0,A1 = 0,A2 = 0,A3 = 0,A4=0,AA0 = 0,AA1= 0,AA2 = 0,AA3 = 0,AA4=0;
unsigned int index = 0,AVG = 0,AAref=0,i,Aref=0;
void main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Stop watchdog timer
BCSCTL1 |= XTS;
do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (i = 0xFF; i > 0; i--); // Time for flag to set
}
while ((IFG1 & OFIFG)); // OSCFault flag still set?
BCSCTL2 |= SELM_3+SELS+DIVM_0; // MCLK= LFXT1
P6SEL = 0x2F; // Enable A/D channel inputs
ADC12CTL0 = ADC12ON+MSC+SHT0_8; // Turn on ADC12, extend sampling time
ADC12CTL1 = ADC12SSEL_1+SHP+CONSEQ_3; // Use sampling timer, repeated sequence
ADC12MCTL0 = INCH_0+SREF_2; // EXTERNAL ref, channel = A0
ADC12MCTL1 = INCH_1+SREF_2; // EXTERNAL ref, channel = A1
ADC12MCTL2 = INCH_2+SREF_2; // EXTERNAL ref, channel = A2
ADC12MCTL3 = INCH_3+SREF_2; // EXTERNAL ref, channel = A3
ADC12MCTL4 = INCH_4+SREF_2; // EXTERNAL ref, channel = A4,
ADC12MCTL5 = INCH_5+SREF_2+EOS; // EXTERNAL ref, channel = A5,end seq
ADC12CTL0 |= ENC; // Enable conversions
ADC12CTL0 |= ADC12SC; // Start conversions
while(1)
{
while ((ADC12IFG & BIT0)==0);
for(index=0;index < Num_of_Results;index++) //code from reading from res and adding the 5 analog inputs
{
A0results[index] = ADC12MEM0; // Move A0 results, IFG is cleared
A0=A0+A0results[index];
A1results[index] = ADC12MEM1; // Move A1 results, IFG is cleared
A1=A1+A1results[index];
A2results[index] = ADC12MEM2; // Move A2 results, IFG is cleared
A2=A2+A2results[index];
A3results[index] = ADC12MEM3; // Move A3 results, IFG is cleared
A3=A3+A3results[index];
A4results[index] = ADC12MEM4; // Move A4 results, IFG is cleared
A4=A4+A4results[index];
Arefresults[index] = ADC12MEM5; // Move A5 results, IFG is cleared
Aref=Aref+Arefresults[index];
}
AA0= A0/Num_of_Results;
AA1= A1/Num_of_Results;
AA2= A2/Num_of_Results;
AA3= A3/Num_of_Results;
AA4= A4/Num_of_Results;
AAref= Aref/Num_of_Results;
A0 = 0;
A1 = 0;
A2 = 0;
A3 = 0;
A4 = 0;
Aref = 0;
AVG = (AA0+AA1+AA2+AA3+AA4)/5;
DAC12_1CTL = DAC12SREF_2+DAC12AMP_7 + DAC12ENC+DAC12IR; // external ref gain 1
DAC12_1DAT = AA0;//AVG;
A0 = 0; //am putting break point here
A1 = 0;
A2 = 0;
A3 = 0;
A4 = 0;
// P1OUT = 0x00;
}
}