Hi,
We are using MSP-GANG430(older version) and the GUI to program MSP430,
when the "Load Image" is pressed the program(txt file) is loaded into the GANG's
internal memory and the status says "successful" displaying checksum value.
We wonder if there is any way to confirm this checksum value with the target MSP430's memory.
The FET-Pro430 has a checksum display window for Source and memory,
is there is any way to crosscheck the checksum value in the GANG430?
i.e. how to make sure the checksum value is proper?
Regards.