Other Parts Discussed in Thread: TEST2
1. It says to terminate pins by setting pin as output by setting P1DIR=0xff; (one of the method)
& then sending zero on it .
Then safer method is to left pin unconnected ?
2. Count down in loops, can someone shed more light on it.
3. I have a program where my required variable can be stored in 14 bits also. So I have done
struct
{
unsigned vol_det : 14;
unsigned vol_rel : 14;
}over;
Other method is to use unsigned int. 16 bits.
Which one's more efficient & power saver. :)
4. Usually MCU gives current in uA/MHZ.