This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI tricky question.

Guru 18625 points

Other Parts Discussed in Thread: MSP430G2452

Hi,

let me try to learn how SPI works in the Launchpad + MSP430G2452. My code (I wanted to do this based on interrupts but I was not having any success so I have to try simpler for now) is the following:

#include <msp430g2452.h>
#include <intrinsics.h>
#include <stdint.h>

uint8_t RXdata;

void main (void) {
uint8_t i;

WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
// pin most energy saving configuration
P1DIR = 0xFF; // All P1.x outputs, it saves energy MSP430x2xx Family User's Guide
P1OUT = 0; // All P1.x reset
P2DIR = 0xFF; // All P2.x outputs
P2OUT = 0; // All P2.x reset

// Pull resistors on unused pins// Enable SDI, SDO, SCLK, msb first, master, enable output, latch data
USICTL0 = USIPE7 | USIPE6 | USIPE5 | USIMST | USIOE;
// Write then read (CPHA = 1 -> CKPH = 0), SPI not I2C, enable interrupt
USICTL1 = USIIE;
// SCLK = SMCLK / 128, clock idles high (CPOL = CKPL = 1)
USICKCTL = USIDIV_7 | USISSEL_2;
// Release USI from reset
USICTL0 &= ~USISWRST;

// SPI transfer
USISRL = 0x46; // this is a READ, a WRITE would be 06
P1OUT |= 0x40; // CS from low to high
USICNT = 8;
for (i = 0xFFFF; i > 0; i--); // Delay
while (!(USIIFG & USICTL1)); // Counter clear?
// this second byte is only important when writing 
USISRL = 0x69; 
USICNT = 8;
for (i = 0xFFFF; i > 0; i--); // Delay
while (!(USIIFG & USICTL1)); // Counter clear?

P1OUT &= ~0x40; //CS from high to low
RXdata = USISRL;

// Enter LPM0 & configure to be able to leave it by interrupt
_BIS_SR(LPM0_bits + GIE);
}

After trying to write some value to the slave's SPI register (same code as above but with opcode 06), when I try to read the destination register, I only obtain 00 in USISRL and I should obtain... 0x69.  :( Argh! I think I've configured all correctly! Below you can see a WRITE transaction as expected by the slave device, and a READ transaction.

My questions are:

  1. Do you think I should employ USI16B in SPI? (16 bit transfers). Or I can success with a similar strategy to my current one? What do you think? :)
  2. As you can see here, the slave is operating on SPI mode = 01 (CHPA = 1, CPOL = 0). This is NOT the most common one in SPI, as far as I know. Since the most common ones are MODE0 and MODE3. Are my thought and source code correct?
  3. Finally... I'm working with the LAUNCHPAD and employing, as typical in MSP430, P1.7 to 1.5 for SPI, and P1.4 as Chip Select. My question is... since P1.6 is also employed for the LED in Launchpad... perhaps this is affecting in my SPI communication? Should I move explicitly a jumper or something to devote 1.6 to SPI or the LED does not affect?

Please let me know your opinion! :) It is my first week with MSP430 so please be benevolent :)

  • The code doesn't set P1SEL.x or P1SEL2.x bits required to select the port 1 pins for the USI module.

    The P1SEL and P1SEL2 registers are cleared at reset which configure the port1 pins as just GPIO.

    See Table 17. Port P1 (P1.5 to P1.7) Pin Functions in the  MSP430G2x52 datasheet SLAS722E for the  P1SEL.x or P1SEL2.x settings required.

  • :(

    Yeah, I have not seen this in any of the examples of the TI resource explorer in CCS5. Is this possible?

    I think I'm missing something like:

    P1SEL |= 0xE0;         // set P1.7, P1.6, P1.5 for SPI functions

    Tomorrow I'm gonna give it a try.

    Thanks a lot.

  • I've resubmitted my question with less questions, since we have helped me a lot to understand some things, even if it is not working yet ;)

    Thanks for everything!

**Attention** This is a public forum