This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430AFE2xx SD24_A Noise

Other Parts Discussed in Thread: MSP430AFE253

I’m using the MSP430AFE2xx Microcontroller 24-Pin Socket Target Board (MSP-TS430PW24) to test the noise performance of the MSP430AFE253 SD24A ADC. I’m not getting the noise performance I would expect from the ADC. I’m getting roughly 10 to 11 noise-free bits (typically 35 – 55 counts of noise) on the upper 16 bit data (total of 65535 counts). Here are the settings I’m using:

Differential input (SD24UNI=0)

Continuous sampling mode (also tried single conversion mode)

Gain of 1 (tried other gains)

Oversampling ratio (OSR) of 1024

Internal analog reference (resulting in an allowable +/- 0.6V max.swing)

Microprocessor is 3V powered by the USB/JTAG (also tried powering externally with a 3.3V battery, removing the JTAG connection, and adding a 470nF bypass cap, but this resulted in little or no improvement)

Pos/neg channel leads internally shorted using SD24INCHx=0x111 and tied to analog ground (also tried externally shorting all input leads)

While there are no performance specs listed for the SD24A, or at least none that I can find, I would expect much better performance from a 24-bit ADC part. I must therefore assume I’m not setting some parameter correctly or not interpreting the output correctly. Any help would be appreciated. 

I did manage to find one source for SD24 noise performance -- in a TI energy tech. presentation for the MSP430F67xx, which includes the SD24 “B” ADC. In that presentation, the SD24B was reported to have a SINAD that approaches 90dB (~15 bits) at an OSR of 1024.

  • SOLVED!

    The modulator clock frequency wasn't being divided down to the proper frequency. Divided by 8 and now I'm getting approximately 15 noise free bits (an SNR of up to ~90 dB, based on pk-pk noise values over an 8 second interval).

**Attention** This is a public forum