Other Parts Discussed in Thread: MSP430F5505
Hi!
I'm using a MSP430F5505 with a 32768 Hz quartz on XT1.
I want to use 2 external load capacitors instead of selecting internal capacitors with XCAP.
Therefore I would clear XTS in UCSCTL6. Is it correct?
What it's not clear to me is if XTS is involved with other stuff or if its only function is to enable/disable internal capacitors. Could anyone clarify this?
Will the power consumption rise selecting XTS?
Best Regards,
Carloalberto Torghele