This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Servo motor control using msp 430 launchpad

hi,I am using the HKSCM9-6 Singlechip Digital Micro Servo (6V) 10g / 1.6kg / 0.07s. I have modified it for full rotation and now its rotating fully but  I have lost the control of the motor.The clockwise and anti clockwise is working fine but I am unable to stop the servo as it is continue going in either in clockwise or anti clockwise direction. I know that we have to pass stop pulse in order to stop the servo but I am unable to find the pulse time for stopping the servo. the motor spec is as given below.

Spec.
Torque: 1.4kg @ 4.8v, 1.6kg @ 6v
Weight: 10g
Speed: 0.09/60deg @ 4.8v, 0.07/60deg @ 6v
Voltage: 4.8v~6v
Plug: JR
my code is as below         Please anybody can help with the code (or) provide any example code. Thank in advance.
#include <stdint.h>
#include <stdio.h>
#include "msp430G2231.h"

#define SERVO_0 650
#define SERVO_180 2350
#define SERVO_COUNT 2
#define SETSERVO(servo, pos) periods[servo].cycle = servopos(pos);

typedef struct period_t_ {
uint16_t cycle;
uint8_t pins;
} period_t;

period_t periods[1 + SERVO_COUNT];
uint8_t period = 0;

void mysleep(uint16_t i);
uint16_t servopos(uint8_t pos);
void initperiod(uint8_t period, uint16_t cycle, uint8_t pins);

unsigned int ShaftAngle;
unsigned int AngleChange;
unsigned int OutputPin;
unsigned int Delay;
unsigned int MaxSteps;
unsigned int StepCounter;

int main(void)
{

WDTCTL = WDTPW + WDTHOLD; /* Stop watchdog timer */

initperiod(0, 20000, 0x00);
initperiod(1, servopos(90), BIT4);

P1OUT = 0x00;
P1DIR |= BIT4; // P1.4
CCTL0 = CCIE;
CCR0 = 65535; // Initial clock interupt
TACTL = MC_1 + TASSEL_2 + TACLR; // Set clock / timing source

_BIS_SR(GIE); // Activate interupts

ShaftAngle = 0; // Whats the current angle of the shaft
OutputPin = 1; // What pin on the IC to raise high
Delay = 50; // How long to wait between each step change
MaxSteps = 10; // How many steps
AngleChange = 10; // Degrees to change shaft position each iteration
SETSERVO(OutputPin, ShaftAngle); // reset to zero

while (1) // Endless Looop
{
// Just wait a moment so we can physically check the servo position (only for testing)
mysleep(5);
for (StepCounter=0; StepCounter <= MaxSteps; StepCounter++)
{
SETSERVO(OutputPin, ShaftAngle);
ShaftAngle+=AngleChange;
mysleep(5);
}

mysleep(5);


// Just wait a moment so we can physically check the servo position (only for testing)

for (StepCounter=0; StepCounter <= MaxSteps; StepCounter++)
{
ShaftAngle-=AngleChange;
SETSERVO(OutputPin, ShaftAngle);
mysleep(5); // Slowly move back to zero position to reduce G force
}
}
}

#pragma vector = TIMERA0_VECTOR
__interrupt void Timer_A_0(void)
{
P1OUT = periods[period].pins;
CCR0 = periods[period].cycle;
if (period ++ >= SERVO_COUNT) period = 0;
}

void mysleep(uint16_t i)
{
uint16_t y, x;
y = i;
while (--y != 0) {
for (x = 0; x < 2400; x ++);
}
}

uint16_t servopos(uint8_t pos)
{
return (uint16_t) ((SERVO_180 - SERVO_0) * (float) pos / 180) + SERVO_0;
}

void initperiod(uint8_t period, uint16_t cycle, uint8_t pins)
{
periods[period].cycle = cycle;
periods[period].pins = pins;
}

**Attention** This is a public forum