I am using Chronos to evaluate the platform for custom wireless control. I have been able to make changes and compile the 433Mhz limited CCS code without any problems so far. When I tried to use simpliciti, I found that the Chronos did not transmit. I tried another Chronos out of the box and it worked just fine. I restarted with an unmodified project and got the same result. I started playing with other functions and found that I could not change the time, it would say loct. I could not unlock the device, either. All of this is being done with the watch is connected to the programming dongle. Is the limited addition supposed to function the same way as a Chronos out of the box? I am using CCSV4.
I also found that if I took another Chronos that had been transmitting to my access point in ACC mode, that as soon as I plugged it into the programming dongle which resets the Chronos, I could not longer make the ACC transmission work regardless of programming.
I tried using the TI access point instead of my own and found that the Chronos was transmitting so it must not have been able to join my network. So whats the difference between an out of the box watch and one that has been reset or reprogrammed with a limited license. Is the radio protocol different?