This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pairing Multiple Chronos Watches with one Access Point :

Hi,
I have a question that can I have multiple chronos wathces to receive data from one AP simultaneously ?

i.e. One A.P transmitting data, and multiple chronos watches receiving it simultaneously, a kind of A.P based message boardcast.

I tried to update the time/date of two chronos wathces through one
Access point, such that I enabled the "Sync" feature of both watches
first and then run the "Chronos Control Centre" on the PC, started AP,
and used "Simplicity Sync" to update date and time on two watches.

However I noticed that only one watch gets its time updated, while on
the other watch the time doesnt update.

I even individually tested and verified both the wathes though A.P. and
the time/date update is always successfull in case of single A.P, single
chronos watch.

is it kind of architecture in which only one A.P and Watch can be paired
with one watch at a time ?

In fact I am at a very basic level of understanding, so I will be very thankful

for any help from anyone, or any opinion.

Thanking in advance,

Regards...

**Attention** This is a public forum