This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2 Series vs Value Line

Other Parts Discussed in Thread: MSP430F2132, MSP430G2453

I am comparing an MSP430 2 series part to a value line (g series) part and was just wondering why the cost difference.

If I have 2 parts that meet all of my criteria why is the g series part so much cheaper?

Is it because it is newer and cheaper for TI to manufacture or is there something else I am missing?

For example. MSP430F2132 vs MSP430G2453

Thanks

  • Hi Jmax604,

    I believe the F2xx families come with DCO calibrated to tighter tolerance than the value line series. Also some of them support high frequency crystals instead of just watch crystals.

    There may be other "niceties" I don't know about, but as far as I know those are the major differences.

    Tony

  • Hello

    the biggest cost savings coming from reduced test conditions. F2xx tested at two Vcc levels, G2xx at one.

    Regards,

    Bernd

  • Jmax604 said:

    I am comparing an MSP430 2 series part to a value line (g series) part and was just wondering why the cost difference.

    If I have 2 parts that meet all of my criteria why is the g series part so much cheaper?

    Is it because it is newer and cheaper for TI to manufacture or is there something else I am missing?

    For example. MSP430F2132 vs MSP430G2453

    Thanks

    Engineering resources can be spent to either make new features or to reduce the cost of an existing product.  In the case of the MSP430 Value Line devices, the emphasis was on lowering the cost as compared to the 2 series equivalent.  As a result, some subtle differences exist between them and their 2 series equivalents (as noted in the discussion above).  If the customer is already using a 2 series part, there may be an engineering cost to migrate to a Value Line part.  However if it is a new design, and devices from either the Value Line or 2 series fit the requirements, I'd say go with a Value Line device.  As a general rule of thumb, I would check to see if a device would fit the requirements in this order: Value Line, 5 series, 2 series. . .

**Attention** This is a public forum