This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need some help with msp430g2553 i2c module :)

Other Parts Discussed in Thread: TMP100

i have problem with using the msp430 with tmp100, my tmp100 has add0=add1=gnd so its address is 0x48 base on the datasheet, i have search some topic related in this forum but i still so confused. I got stuck for several days and really need some help, here is my work

this is function i2c start and stop

void i2c_start(void)
{
    UCB0CTL1 |= UCTXSTT;                    // I2C start condition
    while (UCB0CTL1 & UCTXSTT);             // Loop until I2C STT is sent
}
void i2c_stop(void)
{
    UCB0CTL1 |= UCTXSTP;                  // Generate I2C stop condition
    while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

this is how i init the i2c

void i2c_init(int slave_add)
{
    UCB0CTL1 |= UCSWRST;
    P1DIR |= BIT6 + BIT7 ; // Set SCL, SDA  as Output
    //P1REN |= BIT6 + BIT7; // enable Pull-Ups or down on SCL and SDA
    //P1OUT |= BIT6 + BIT7; // Set Pull-Ups on SCL and SDA
    P1SEL |= BIT6 + BIT7;                     // Assign I2C pins to USCI_B0
    P1SEL2|= BIT6 + BIT7;                     // Assign I2C pins to USCI_B0
    UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;
    UCB0CTL1 = UCSSEL_2 + UCSWRST;            // Use SMCLK, keep SW reset
    UCB0BR0 = 12;                             // fSCL = SMCLK/12 = ~100kHz
    UCB0BR1 = 0;
    UCB0I2CSA = slave_add;                         // Set slave address
    UCB0CTL1 ^= UCSWRST;                     // Clear SW reset, resume operation
}

this is how i config and read the temperature

void i2c_config_tmp100(void)
{
    UCB0CTL1 |= UCTR;  // I2C Transmitter
    i2c_start();
    UCB0TXBUF = 0x01;  // POINT REGISTER = 01 => CONFIGURATION
    while(UCB0TXIFG==0);
    UCB0TXBUF = 0x60;  // SET THE RESOLUTION TO 12 BIT (0.0625 CELCIUS DEGREE)
    i2c_stop();

    UCB0CTL1 |= UCTR;
    i2c_start();
    UCB0TXBUF = 0x00;  // POINT REGISTER = 00 => TEMPERATURE REGISTER
    i2c_stop();
    UCB0CTL1 ^= UCTR;  //  receiver mode

}

void i2c_tempread_tmp100(void)
    {
    i2c_start();
    data_tmp100[1]=UCB0RXBUF;//
    while(UCB0RXIFG==0);
    data_tmp100[0]=UCB0RXBUF;//
    i2c_stop();
    }

void i2c_lcd_tmp100(void) => this function is used to put the raw temperature on the lcd
{
    lcd_gotoxy(0,1);
    data_tmp100[2]=( (data_tmp100[1]<<4) | (data_tmp100[0]>>4) );
    lcd_putnumber(data_tmp100[2]);

}

in the main.c, after init the lcd, the i2c module, i call the function i2c_tempread_tmp100 after every 2s

 this is my first post in this forum, if i did something wrong, please tell me :P

**Attention** This is a public forum