I am running Windows 7 and am using CCS 5.1.1 to connect to an MSP-FET430UIF which is in turn connected to a privately designed board containing an MSP430F5529. I have been getting the above error message when I try to connect. A search on this forum came up with a solution to someone else's similar problem, where they were using an MSP430BT5190. The solution was provided by Andreas Dannenberg on 18-Jan-2012 as a zip file: SP_MSP430BT5190_Tue001_17_2012__11_16.zip. The zip file is dated/authored 01/17/2012 Florian Berenbrinker. Reading the enclosed pdf and txt files I get the distinct impression it will not work for other MSP430 devices. Is there a more general solution that works for all MSP430 devices and where can I get it? Regards, Harry.