This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2370 Flash Memory Write Errors

Hello.

I have some trouble when writing in Flash Memory . Data are not always correctly written.

Flash segment is correctly erased before writing datas.

Instead of writing my code here,  here is a screenshot.

As you can See at 0x800F , I have 0xADE6  Instead of  0xAD05 :

Errors seems to appears randomly ( not always at the same address)

(Bigger image here :

http://img51.imageshack.us/img51/2920/screenshot131.png

)

 

 I do not know what can be the problem.

Any Idea ?

Thanks

 

 

**Attention** This is a public forum