Hello All,
I was wondering if anyone else has encountered a similar problem to mine. The CMA3000 is programmed to be in the 400Hz ODR mode. I then have the device attached to a shaker for calibration. The shaker is oscillates at a 4Hz sine wave. To me this means I should have 100 data points per 4Hz cycle. Unfortunately I have 10 data points per 4HZ cycle. This indicates that the CMA3000 ODR is programmed at 40Hz. Not sure whats going on. As a side note I pulled the data into matlab and took an fft at using 40Hz sample rate and also tried 400Hz sampling rate and sure enough the 40Hz is spot on. Like I said I was wondering if this is a known issue, or something I may be missing. Thanks in advance.